SEM-SAFE® high-pressure water mist system High-pressure water mist is water that, at a high-pressure of 100 bar, creates a fine mist. The fine water mist evaporates very quickly and the resulting steam starves the fire of oxygen, suppressing it. At the same time, the water evaporation creates the most efficient form of cooling. In this way, the fire is extinguished both by oxygen suppression and cooling, providing the advantages of both water and gas-based fire fighting. Danfoss has been working with high-pressure water mist right from the start. This revolutionary new system is finding its way into more and more application areas, offering an efficient system that is environmentally friendly as well as harmless to users. Approval levels and experience We have already seen fires being almost instantly extinguished by the system after its release, thus saving repair costs and off-hire periods. High-pressure systems only create a high pressure during extinguishing. High pressure water mist will cool the areas around hot metal surfaces and the water mist evaporates before it reaches the hot metal. In this way, shock cooling and changes in metal structures can be avoided. The SEM-SAFE® system is approved by all major classification societies. Filter Unit UCP Pump Unit Reservoir tank Set @ 115 Barg UCP PI-2100 PI-2100 Water supply USP USP UCP ZSO USP Skid limit Typical arrangement of section valves in an engine room. ® Danfoss Semco A/S · Member of the Danfoss Group · Middelfartvej 9 · DK-5000 Odense · Denmark Tel. +45 7488 7800 · E-mail semsafe@danfoss.com · www.semsafe.danfoss.com Danfoss Semco A/S can accept no responsibility for possible errors in catalogues, brochures and other printed material. Danfoss Semco A/S reserves the right to alter its products without notice. This also applies to products already on order provided that such alternations can be made without subsequential changes being necessary in specification already agreed. All trademarks in this material area property of the respective companies. SEM-SAFE® logotype is trademark of Danfoss Semco A/S. Danfoss logo type is trademark of Danfoss A/S. All rights reserved. © Copyright Danfoss Semco A/S | 2018.09
Download PDF file
Archive