SEM-SAFE® high-pressure water mist system The SEM-SAFE® water mist system was installed at the Multifunctional Platform Supply Vessel (MPSV) M/V Olympic TBN in 2008. The type of fire protection installed on the 4,900 tonnes deadweight vessel is total flooding in main engine room, inclu-ding bilge and casing plus switchboard room. In addition, local protection systems have been installed for each of the four main engines, fuel oil separator, boiler and incinerator. In total, 115 nozzles have been installed. The 2,000x900mm pump unit consists of three main PAH 63/22kW pumps and one standby with a capacity of 318 l/min. Emergency change over box according to DNV rules. The bottle bank has a capacity of 1 minute water discharge in case of black out. ® Danfoss Semco A/S · Member of the Danfoss Group · Middelfartvej 9 · DK-5000 Odense · Denmark Tel. +45 7488 7800 · E-mail semsafe@danfoss.com · www.semsafe.danfoss.com Danfoss Semco A/S can accept no responsibility for possible errors in catalogues, brochures and other printed material. Danfoss Semco A/S reserves the right to alter its products without notice. This also applies to products already on order provided that such alternations can be made without subsequential changes being necessary in specification already agreed. All trademarks in this material area property of the respective companies. SEM-SAFE® logotype is trademark of Danfoss Semco A/S. Danfoss logo type is trademark of Danfoss A/S. All rights reserved. © Copyright Danfoss Semco A/S | 2018.09
Download PDF file
Archive