Marine application | SEM-SAFE® high-pressure water mist system Reliable fire fighting in accommodation areas Danfoss Fire Safety A/S As one of the world’s few manufacturers, Danfoss can offer protection of your accommodation areas with a true highpressure water mist system approved to IMO A 800 and IMO resolution MSC/circ. 265. The SEM-SAFE® high-pressure water mist system has an advantage over traditional sprinkler systems in that it uses only approx. 20% of the amount of water to cover a given area. In addition, reduced pipe dimensions mean a considerable reduction in weight and allows installation in smaller spaces. As a consequence of the small pipe dimensions, installation is very easy and Danfoss has developed a fitting system making installation even easier. If you experience accidental releases in public areas or cabins, the very low water quantity means that water damage is limited. The nozzles used in accommodation areas are usually the closed type with a glass bulb that breaks at a set temperature. On standby, the system maintains only a low pilot pressure. In addition, it is possible to integrate total flooding and local application fire fighting system to the same pump unit. www.semsafe.danfoss.com
Share
Print
Download PDF file
Archive