Optimum fire protection The SEM-SAFE® high-pressure water system provides instant fire suppression by releasing micro-droplets of water directly onto the affected area. These droplets form an ultra-fine mist, which tackles the fire in two ways; by cooling the flames and by simultaneously starving the fire of oxygen, thereby preventing re-ignition. High- pressure water mist is highly effective in the fight against fire, providing excellent protection against heat damage. Intelligent design minimises water damage A key benefit of the SEM-SAFE® system is that the mist is highly targeted at the source of fire. If a fire is detected and confirmed by the alarm system, a section valve will open immediately, allowing water to flow into the otherwise dry distribution pipe network. No other valves will open, ensuring that the mist is deployed exactly where it is required and nowhere else. Furthermore, the high-pressure water mist produces a high level of atomisation, which means water droplets are exceptionally small; which further reduces the risk of water damage. Bespoke design, backed up by local support Key to Verne Global’s decision to deploy the SEM-SAFE® system was Danfoss Fire Safety’s reputation for excellent customer support. With operations across the globe – including in Iceland – the Verne Global team had peace of mind that the deployment would be closely managed; vital as this was the first of deployment of its type in the country. The on-the-ground team was ably assisted by the specialist experts at the Danfoss Fire Safety headquarters in Denmark, which created a bespoke design, alowing the Verne Global team to visualise the entire system prior to the deployment. Danfoss Fire Safety’s system is the ideal fit for our data centre. Not only is it rigorously and independently tested to suppress fires, it is designed to minimise water damage too, which is crucial considering the value of the IT equipment located within our ultra-high density pods. Local presence was also an important factor in us choosing the company as a strategic supplier. This was a mission-critical deployment for Verne Global, so having a highly-professional team on the ground – backed up with first-class support in Denmark – was immensely reassuring.” Helgi Helgason Managing Director, Verne Global, Iceland Cost efficient, scalable design For data centres, efficiency is of paramount importance, and this is particularly the case for Verne Global, which specialises in providing sustainable solutions. The SEM-SAFE® system is highly efficient. Its pump unit has a compact design, while – unlike gas suppression techniques – the system can be used multiple times, doesn’t require any expensive refills and is virtually maintenance- free. In the event of a false discharge, the system can be stopped and will be immediately ready for re-use; a feature not possible with alternative solutions. It also comprises high-quality, durable stainless-steel pipes that further reduce the system’s total cost of ownership. Finally, it is easy to scale and configure; ideal as Verne Global continues to bring more ultra-high density data centre pods online. Aligned with environmental goals Organisations often locate their equipment at the Verne Global campus because it is 100% powered by geothermal and hydroelectric electricity. The SEM-SAFE® system has been designed with the environment in mind. Lubricated by water rather than oil, there is zero risk of contamination, while the system also boasts low power and water consumption. SEM-SAFE® advantages The SEM-SAFE® system comprises a high-pressure modular pump unit, section valves, piping and water mist nozzles. With small pipe dimensions, large coverage and minimal water consumption, SEM-SAFE® high-pressure water mist is a reliable choice to protect data centres against fire, offering: Reliable fire suppression Protection for IT equipment Compatibility with fresh air cooling Low energy consumption No refill costs Maintenance-free pumps FM accreditation About Danfoss Danfoss is a Danish multinational company, that manufactures products and services used in cooling, heating, air conditioning, fire safety, drives, power modules and much more. With over 28,000 employees and operations in over 100 countries, Danfoss is fully committed to developing sustainable and climate friendly solutions for greener cities and more efficient district energy networks. ® Danfoss Fire Safety A/S · Middelfartvej 9 · DK-5000 Odense · Denmark Tel. +45 7488 7800 · E-mail firesafety@danfoss.com · www.semsafe.danfoss.com Any information, including, but not limited to information on selection of product, its application or use, product design, weight, dimensions, capacity or any other technical data in product manuals, catalogues descriptions, advertisements, etc. and whether made available in writing, orally, electronically, online or via download, shall be considered informative, and is only binding if and to the extent, explicit reference is made in a quotation or order confirmation. Danfoss cannot accept any responsibility for possible errors in catalogues, brochures, videos and other material. Danfoss reserves the right to alter its products without notice. This also applies to products ordered but not delivered provided that such alterations can be made without changes to form, fit or function of the product. All trademarks in this material are property of Danfoss A/S or Danfoss group companies. Danfoss and the Danfoss logo are trademarks of Danfoss A/S. All rights reserved. © Copyright Danfoss Fire Safety A/S | 2021.09
Print
Download PDF file
Archive