A safer tomorrow starts with SEM-SAFE® It is crucial that high-rise buildings are fully and properly equipped to handle a fire situation. In high-rise buildings, the access for the fire fighting crew can be very difficult, especially on the last levels of the buildings. Also evacuating people presents challenges and limitations. Having a fixed high-pressure water mist system installed in high-rise buildings can make the fight against fire more efficient, with the ultimate goal of saving lives and limiting property damage. Imagine a fire fighting system that can put out the fire in seconds, with minimal consumption of water, giving the best possible protection. With SEM-SAFE® – the unique high-pressure water mist system from Danfoss – that is what you get. By using pure water, the high-pressure water mist technology used by the SEM-SAFE® system is harmless to humans and environmentally friendly. Its reliability and efficiency has been successfully proven in rigorous fire tests. 4 Danfoss Fire Safety A/S · High-rise buildings
Download PDF file
Archive