SEM-SAFE® high-pressure water mist system The project has been the result of close collaboration between Danfoss, Kemp-Lauritzen (official Danfoss distributor in Denmark) and consulting engineering company, DNU Rådgivergruppen. The advantages of a high-pressure water mist system were solidly confirmed. All fire protection requirements were satisfied by choosing a SEM-SAFE® high-pressure water mist system. Fire safety consultants Kenneth Jaquet and Bertel Kjeldsen, Rådgivergruppen DNU I/S states: “By installing a high-pressure water mist system at The New Aarhus University Hospital (DNU), we have selected the optimal technology when it comes to protecting the building, its fixtures and equipment in the event of a fire. This technology also allows for considerable savings in terms of building components. Simplex CEN micro nozzles and VdS drilled nozzles have been chosen. The CEN nozzle has a large spacing of 5.5 meter, with its wide spray angle and the specially designed spray pattern. Upon project completion, a total of 30,000 nozzles will be installed. The high-pressure water mist system has provided a high level of architectural freedom, such as the ability to mount nozzles in the moulding in corridor areas so that the ceiling can easily be removed to provide access to technical installations during service visits. High-pressure water mist has excellent fire suppression properties, including the capture of soot particles, strong reduction of radiant heat and rapid lowering of the temperature to acceptable levels. Fire is controlled efficiently, while water consumption and water damage is kept to a minimum. In case of system activation due to a fire, the clean-up is faster and there is minimum business interruption and impact on patient care. The benefits of SEM-SAFE® The benefits of SEM-SAFE® high-pressure water mist system are many in comparison with traditional sprinklers. The most important being the economic advantage, as SEM-SAFE® is a money saving solution. For DNU more than 11 million Euros were saved with SEM-SAFE® due to lower costs for building structure and design. At DNU, the technology has also allowed planners to replace widelyused automatic fire doors in service corridors with high-pressure water mist curtains, which are a more reliable and operations-friendly solution. The building has also been equipped with high-pressure hose reels, which can be used by emergency response teams in the event of a fire. The high-pressure hose reels are an integrated part of the highpressure water mist system, thus avoiding the need for a separate pipe network for traditional hose reels. In a hospital construction with limited space for technical installations, the high-pressure water mist system is the optimal choice when using smaller and fewer pipe sizes, as it provides the utmost flexibility.” The superior cooling features of the SEM-SAFE® water mist system make it the perfect choice for glass facades, as it removes the risk of thermal stress cracks associated with traditional sprinklers. Usually a lot of isolation material has to be used for vents in order to prevent any hot air being transported. With SEM-SAFE® this is avoided and significant savings are made. The SEM-SAFE® system is characterized by small pipe dimensions and fewer nozzles, which results in considerable reduction of installation time and cost, impossible to achieve with a traditional sprinkler system. The small pipe diameters make the system easy to integrate with other installations in a hospital. It is an optimal solution for modern hospitals as well as being highly suited for retrofitting existing buildings. The innovation behind SEM-SAFE® has allowed for water curtains to replace traditional fire doors. ® Danfoss Fire Safety A/S · Middelfartvej 9 · DK-5000 Odense · Denmark Tel. +45 7488 7800 · E-mail firesafety@danfoss.com · www.semsafe.danfoss.com Danfoss Fire Safety A/S can accept no responsibility for possible errors in catalogues, brochures and other printed material. Danfoss Fire Safety A/S reserves the right to alter its products without notice. This also applies to products already on order provided that such alternations can be made without subsequential changes being necessary in specification already agreed. All trademarks in this material area property of the respective companies. SEM-SAFE® logotype is trademark of Danfoss Fire Safety A/S. Danfoss logotype is trademark of Danfoss A/S. All rights reserved. © Copyright Danfoss Fire Safety A/S | 2019.06
Download PDF file
Archive