Case story | SEM-SAFE® high-pressure water mist system CitizenM London Shoreditch Hotel An innovative hotel offering its guests affordable luxury – all protected with SEM-SAFE® high-pressure water mist mist for fire fighting Danfoss Fire Safety A/S The hotel has a great location in Shoreditch, East London, England, in a lively area that is becoming more and more known for fashion and vibrant cultural events. In line with the transformation of the area, CitizenM London Shoreditch promotes the philosophy of affordable luxury. The hotel was built on the location of a former railway viaduct. The former steel structure had a significant impact on the hotel’s structure. As a result, CitizenM was built to the exact proportions of the old viaduct. The lobby has a unique balcony that overlooks the tube train situated on top of the building from across the street. Building description CitizenM London Shoreditch is an 11-storey hotel. The 14,000-square-metre, mixed-use area comprises 216 bedroom pods and 24 ironing/linen rooms that are stacked above a concrete deck and, in themselves, the pods form the main structure of the building. The lobby is created to give the impression of a very open space, with a comfortable lounge area and bar, designed in a modern and colorful fashion. All is protected with SEM-SAFE® high-pressure water mist for fire fighting from Danfoss. www.semsafe.danfoss.com
Download PDF file
Archive